I have simulated the LT8636 step-down DC/DC converter in LTSpice (see attached), with the following conditions:
- Vin = 28V
- Vout = 5V
- Iout = 1.96A
- Fsw = 1MHz
- Inductor (L) = 2.7uH

However, I am noting a couple of discrepancies and concerns:
-
The total efficiency in my LTSpice simulation is ~89%, which is notably lower than the ~95% efficiency predicted by LTpowerCAD & datasheet under the same conditions.
-
I also observe very large current spikes on the Vin1 pin (the high-side FET) in the simulation.

Could someone help explain:
-
Whether those current spikes are just artifacts of the simulation, or if they represent something physically realistic?
-
Why there is such a significant difference in efficiency between LTSpice and LTpowerCAD, and which of the two would you generally trust more for estimating actual, real-world performance?
Thank you very much for any insights.
Fedep