Hello,
I use two LT1054IS8#PBF to generate a voltage of -11V from a +12V but which can deliver 130mA max.
The two LT1054IS8#PBF are wired in parallel.
I have a 1ohm ballast resistor on each output. Nevertheless, I have a regulator that heats up more than the other. I deduce that there is only one of the two who is cutting from the current. But I don’t understand why.
If you have an idea.
Thank you in advance