Post Go back to editing

Inductor Sizing

Category: Hardware
Product Number: LT8708

Hi all,

I'm currently trying to use the LT8708, in order to power a board. I'd like it to have a nominal behavior (buck/forward mode) where Vin is between 32 and 60V and Vout is 12V. But under certains conditions it should be able to switch to reverse mode (boost mode) with Vout becoming the "supply" voltage (still 12V) and Vin being supplied by the LT8708 to a level of 32V.

Following datasheet to chose the different components of the sub-circuit, I've reached a part where I'm selecting the Inductor. At this time there's a formula to compute the minimum inductor in boost mode :   

I was wondering if, in my case, Vout (of the datasheet) would be my Vin and Vin my Vout or not. In that case I can compute L because Vout = MyVin = 32V and Vin = MyVout = 12V and condition Vout greater than twice is reached but if I don't switch then Vout is not twice Vin and I should not calculate L ?

Have a nice day,

Will.

  • Hello William,

     

    Since you are designing for Buck mode only, use the Buck inductor calculation. This is provided in page 33 of the datasheet. Additional information also mentioned about adjusting some values in case the calculated inductance is too large or negative. I would recommend at the same time to design your circuit with the aid of LTpowerCAD as the controller is available for this design tool. Would be easier for your  to tweak some values and see your designs behavior. 

  • Hello Tonie,

    Thanks for the answer.

    I'm not designing for buck mode only, I have two "modes" when my main battery (Vin) is above a certain threshold, I'm in buck mode. When this same main battery is under a certain threshold or missing, Vout (12V generated by an auxiliary battery) provide 32V to Vin through LT8708, boost mode.

    I'll also take a look at LTpowerCAD at the same time.

    Have a nice day,

    Will.