Post Go back to editing

VSYS Voltage in backup mode when boost converter disabled (/BSTEN>1.2V)

Category: Hardware
Product Number: LTC4041

Hello,

with LTC4041, In backup mode (no input power supply)  with /BSTEN>1.2V   (Backup Boost Converter disabled), is the system powered by  the supercapacitor without boost voltage or  is it completely isolated from the supercapacitor?

Same question when the LTC4041 is in shutdown mode?

Best regards.

Sylvain

Edit Notes

subject modify
[edited by: FLOWBIRD at 8:40 AM (GMT -4) on 31 Oct 2025]
  • With Vin removed and /BSTEN tied above 1.2V (boost converter disabled), there is no longer a path from the supercapacitor to the Vsys node so Vsys is not powered from the supercapacitor.

    The same is also true in shutdown mode (where /CHGEN = /BSTEN >1.2V). The input and supercap are disconnected so there is no path to Vsys.

  • Thank your for your answer!

    Two more questions.

    1. With VIN removed, is it mandatory to connect /CHGEN and /BOOSTEN above 1.2 V (shutdown mode) to get the lowest power consumption, or is it enough to connect /BOOSTEN above 1.2 V and keep /CHGEN connect to GND.

    2. When 2 mosfets are used  (OVP protection), could we use it  as a power switch to disconnect Vin from VSYS by using the shutdown mode?

    In therorical point of view it seems to be ok, but   it seems that igate signal is very weak. Moreover what will be  the inrush current caused by CSYS capacitor when the  mosfets will be switched? 

    Have you got some feedback of this usage of the IC?

    Best Regards

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.