Post Go back to editing

Clarification on MAX77857 Buck-Boost Output Current Capability

Category: Datasheet/Specs
Product Number: MAX77857

Hi there,

We are facing an issue with the MAX77857 Buck-Boost converter. Please find the summary below:

  1. Input Voltage: 3.4 V – 13 V (Battery range: 3.4 V – 4.2 V)
  2. Output Voltage: 5 V fixed (set by internal resistor)
  3. Output Load: Up to 4 A

During testing, we observed that when the load current increases beyond 1.5 A, the output voltage drops significantly, fluctuating between 2 V and 5 V. We have tested two separate boards (each with a different IC) under varying loads and observed the same voltage drop issue.

For your reference, we have attached the test results and the MAX77857 schematic.

Kindly review and suggest the next steps to resolve this issue.

 XLSX

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.