Post Go back to editing

Random Failures in Latest Build

Category: Hardware
Product Number: ADM7171

We have been using the ADM7171 for couple of years now, all low volume runs <60 pcs per run, and have never had any issues.  On our most recent run we are now seeing, as far as we can tell, random failures of the ADM7150ACPZ-3.3.  We have six of these supplies per board and the failures are random within and between boards.  There is no systematic failure we have been able to identify and as mentioned we have been using this part with these components for a couple of years and have never once seen a failure.

All failures have been observed off of the assembly line.  Occasionally we have seen a failure after rework when using a part from the same batch, currently these parts are on order at all suppliers so we have not been able to purchase more.

The failure is generally been observed as an output voltage of ~1.3 V to 1.4 V instead of the fixed 3.3 V.

We have had a change in manufacturers on the most recent run switching to a vapor phase process instead of conventional reflow.  No other parts on the board have experienced failures, off of the assembly line.

The parts purchased this run were from a recommended distributer, Arrow.

  • Hello Sam, 

    Thank you for sharing details. 

    Could you please confirm whether you are using ADM7150 or ADM7171?

    Just to clarify:

    ADM7171 is a 1A device 

    ADM7150 is 800mA LDO

    Let me know which one you are working with so I can assist you further.

  • I made an error on the post, we use both supplies on our board but the chip we are having troubles with this run is the ADM7150 chip.

  • Thanks for confirming you're using the ADM7150.
    Given that this design has been in place for a couple of years and the device was ordered through an ADI-authorized distributor, Arrow; suggests the issue might be related to one of the following:

    • Changes in the Bill of Materials (BOM)
    • Board assembly process
    • Manufacturing variations

     

    Here are few things I would recommend:

    1. Check and confirm no change in BOM for circuitry associated to ADM7150
    2. For soldering please refer to JEDEC standard J-STD-020 :

        https://www.jedec.org/

      For LFCSP packages please see our guide at this link:

       https://www.analog.com/en/resources/app-notes/an-772.html

      For SOIC-EP packages please see attached guide 

       PDF

    3. You can also X-ray your device to confirm you have enough coverage

       

      4. Check if the IC is getting correct input voltage at Vin, are you measuring correct voltage on Vreg

        

     

  • 1.a Schematic was unchanged around all 6 supplies from the last run of boards. 

    1.b The capacitor used on the BYP pin changed from TCSOPL1A226M8R to T529P226M010AAE200.  Both caps are 22uF tantalum caps, 200 mOhm ESR, and 0805 footprint.  The only difference between the 6 on the board is 2 supplies have their enable pin controlled while the other 4 have enable tied to VIN.  Failures have been observed for both cases.

    1.c Gerbers were checked for one of the supplies, that had experienced a failure, and no difference could be seen between previous working runs and the latest board with failures.

    2. I have reviewed the Board Design section and all recommendations are implemented.  I have handed off to the manufacturer for input.

    3. Will follow up with manufacturer and update post after.

    4. See image below.  All 6 supplies are fed from a 5V DC-DC regulator.  Some are working and some are not working from the same rail.  It has been verified to be correct at 4.97V.

  • Update:

    Regarding question 2

    Yes, the boards have been assembled in compliance to this standard. If the maximum applied temperature is of interest—it was 238°C. According to Table 4-2 (J-STD-020C Proposed Std Jan04.pdf), packages with a thickness of less than 1.6 mm (which is the case for the ADM7150) can withstand a peak temperature of 260°C for 60–150 seconds (see Table 5-2).

    Regarding question 3

    Yes chips were X-rayed and sufficient solder was observed

    We ordered an Eval kit for the ADM7150 to check supplies that had failed and found the following. Chips that failed require a much larger voltage drop to work than the datasheet specs.  Nominally we have a 5V input to the ADM7150 in our design and are observing anywhere from 0 V to 1.5V on devices that are not working.  On the evaluation kit the bad devices are able to regulate 3.3 V with a load of 80 mA but at a load of 680 mA it requires 6 V.  The datasheet specifies in the worst case scenario the minimum dropout required is 1 V.  What we are observing is that a drop out of > 2V is required to regulate properly on bad devices.

    This chip is currently unavailable everywhere... Was there a known bad batch?

  • Thanks for providing information on soldering and xray. I have few questions related to: 

    Nominally we have a 5V input to the ADM7150 in our design and are observing anywhere from 0 V to 1.5V on devices that are not working. On the evaluation kit the bad devices are able to regulate 3.3 V with a load of 80 mA but at a load of 680 mA it requires 6 V.

     

    1. The device you tested on evaluation board : what is the measured Vin and Vreg? 
     
    2. With no device soldered on your board, what do you see on Vin node of ADM7150?
    3. Can you provide schematic of your design showing all connections of ADM7150 and corresponding external components
     
     
     
  • 1. See table of results from evaluation board, the part used on the evaulation board was an ADM7150ACPZ-3.3.  Iout was varied using a resistive load.  These results were very similar for 4 separate chips that had "failed" on our board. 

    Vin (V) Vreg (V) Vref (V) Vout (V) Iout (mA)
    6 3.9 3.3 3.3 680 (~5 ohm)
    5.5 3.9 1.8 1.8 270 (~5 ohm)
    4.3 3.9 0 0 (no load)
    4.5 3.9 3.3 3.3 80 (~40 ohm)

    NOTE: We are in the process of putting chips from the reel, that have not been assembled on our board, onto the evaluation board to confirm if the failures are observed off the reel or only after they have been assembled on our board.

    2. On our board we see 5 V at Vin with all parts populated and 5V at Vin with no parts populated.

    3. Snippet of one of the schematic for one of the ADM7150ACPZ-3.3 on our board. This portion of the schematic has been unchanged in 2 years and we have seen this supply fail on more than 1 board but not on all boards this run, of 4 total boards in the first run.

     

    C809, C923, C732: Taiyo Yuden, LMK316AB7106MLHT

    C808: Kemet, T529P226M010AAE200 (note this is a 22 uF cap instead of 33 uF as shown in the schematic)

    C877: Taiyo Yuden, LMK105BJ105KVHF

  • Additional testing on our board, good LDO vs. bad LDO.

    Good LDO

    Note: Ven is 3.3 V here and Vin (5V) is not shown. Vin is the same 5V power rail for both the good and bad LDO.

    Channel 1 -> Ven (yellow)

    Channel 2 -> Vout (blue)

    Channel 3 -> Vref (red) 

    Channel 4 -> Vreg (green)

    Bad LDO

    Channel 1 -> Vin / Ven (yellow)

    Channel 2 -> Vout (blue)

    Channel 3 -> Vref (red) 

    Channel 4 -> Vreg (green)

  • Please check connection (soldering) for both input and output capacitors

  • Please check connection (soldering) for both input and output capacitors