Post Go back to editing

Can the LT8210 be used in series with other LT8210 circuits?

Category: Hardware
Product Number: LT8210

Hi,

Can we use the LT8210 in series with other LT8210 to make a regulated high voltage rail from many batteries? Like the diagram below. We will include schottky diodes so the load current will bypass the LT8210 when its off or when its battery is disconnected.

The goal is to make modular 48V batteries that can be used in series to make high voltages.

The ABS MAX lists -0.3V on VOUT, SNSP2, SNSN2, and this would put -0.8V there. We could put series resistors to limit the current flow.

Thanks

Steve

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.