Post Go back to editing

Vin range extended

Category: Hardware
Product Number: ADP1074ACCZ, ADP1074, ADP1074

Hi, I need an isolated PSU with an input of 9 to 60 V and an output of 12 V at 6 A. Is it possible to use the ADP1074ACCZ in forward mode with the same transformer across the entire input range?
An alternative, if simpler, could be a 5 V, 15 A output.
Many thanks.

Edit Notes

added 5V 15A output variation, changed Vin min from 6V to 9V
[edited by: LucBuc at 1:45 PM (GMT -4) on 25 Oct 2025]