Post Go back to editing

LTC4358: Preventing current backflow

Category: Hardware
Product Number: LTC4358

Hi. I'm looking at ways to prevent reverse flow of current to a power supply. One solution I'm looking at is the LTC4358. It seems appropriate for the range of voltages I plan to use it for, from 10 to 25 volts max ideally. However, in simulation, I have an issue with its functionality with a high capacitve load. 

When the input voltage suddenly drops from its max input voltage to 0, there is a reverse current spike of roughly 1 amp for a duration of a few nanoseconds, roughly 5-6 nanoseconds. The datasheet says that the diode should turn off within 500 ns, so this seems to be expected, but is there a way to prevent this sudden spike? I'm concerned that a sudden, short spike like this can damage my power supply.

6232.test03-LTC4358.asc

Thread Notes

  • Some reverse current is needed to generate the negative VDS to trigger fast turn-off.
    Since the LTC4358 uses an integrated NFET, you cannot change the reverse recovery performance.
    If you were using an ideal diode with an external FET like the LTC4359, you could switch to a higher RDS(ON) FET to reduce the amount of reverse current.

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.