I want to understand the datasheet specification.

Vcontrol pin and IN pin both have voltage rating +40V with respect to Vout and not ground ?
If true then I can connect +55V on Vcontrol pin and IN pin get output of +50V.
KCC's Quizzes AQQ305 about a mutual exponentiation equation
1. Quote of the month: "A train station is where a train stops. A bus station is where a bus stops. I have a work station on my desk, so..." - unknown
2. Quiz AQQ305 about finding a mutual exponential equation
Good luck, and try to be among the
View All
October Monthly Blog Quiz! Read the blog, take the quiz, and you could win a gift card
Finding Your Circuit Chi — EMC Quiz!
Think you know EMC? Test your knowledge with our 5-question quiz!
Read the blog first, then take the challenge: Finding Your Circuit Chi
Every current flowing creates electromagnetic fields.
Strong EMC design
View All
LT3080
Recommended for New Designs
The LT3080 is a 1.1A low dropout linear regulator that can be paralleled to increase output current or spread heat in surface mounted boards. Architected...
Datasheet
LT3080 on Analog.com
I want to understand the datasheet specification.

Vcontrol pin and IN pin both have voltage rating +40V with respect to Vout and not ground ?
If true then I can connect +55V on Vcontrol pin and IN pin get output of +50V.
The -0.3V Absolute Maximum Rating for the LT3080 that you show in your image indicate that the LT3080 has parasitic diodes from OUT to IN and OUT to VCONTROL. I draw the parasitic diodes on the LT3080 block diagram in the image below. You can make a 55VIN to 50VOUT LT3080 circuit, but you have to clamp IN=VCONTROL to OUT and also IN=VCONTROL to SET so the 40V Abs. Max. ratings are not exceed. I talk more about a circuit for arbitrarily high output voltages in this Engineer Zone post. The title of the EZ post is "Is it possible for the LT3081 to generate 40V from 45Vin if the potential difference from Vin to Vout is within 40V?"

Thanks,
I still have doubt. Should I place clamping diodes between VIN to OUT and VIN to SET pins?