Post Go back to editing

LTC4221 Not working correctly on custom board

Thread Summary

The user implemented the LTC4221 on a custom board, which works correctly in LTspice but fails on the board when the 12V input on channel 2 exceeds 5.9V, causing a fault and auto retry mode. The final answer suggests checking the PCB design and soldering for issues. No specific URL or additional details were provided.
AI Generated Content
Category: Hardware
Product Number: LTC4221

Hi there..

I have implemented LTC4221 of my custom board as in LTspice simulation. It is working correctly in LTspice but not on my board.

The problem is 12V input on channel 2 causing fault as i can probe on oscilloscope. it is working only till 5.9V input and above that triggering fault and LTC4221 goes into auto retry mode. 

Below is schematic (also same on my board)

I appreciate for any help!

With regards

Jitu

  • Jitu,

    I don't see anything wrong with the LTspice circuit that you have posted. I can only suggest that you carefully check the design of your custom PCB and the soldering.

    Regards,

    JayBee

  • The LTC4221 IC is tripping its overcurrent or fault threshold when the input on Channel 2 exceeds 5.9 V. This suggests a configuration or a PCB layout issue and not the the IC itself. In your testing ensure that the VCC2 of the channel 2 is not greater than the VCC1 of the channel 1, as that might trigger the fault and LTC4221 would go to auto retry mode. Another thing is the layout. Try and follow the layout guide in the datasheet. Also ensure the sense resistors are kelvin connected in the PCB, so the IC does not see overcurrent at higher voltage.