Post Go back to editing

Two-switch flyback

Category: Hardware
Product Number: LT3748

Hello,

I'm evaluating the use of LT3748 flyback controller for a two-switch flyback topology and I have some concerns. 

To drive the two switches, I'm considering either a pulse transformer or bootstrap half-bridge driver but the concerns comes from the RFB pin and the no-opto control scheme. 

On the primary side there is a 48V rail and we will transfer the power to 4 outputs as a pre-regulated output for several CCCV converters. Output power is 4x25W and output voltage can swing from 15 to 32 [V] considering cross-load regulation.

* Can I expect problems with the boundary operation mode due to the change in the reflected voltage? 

* Do you expect any problems related with the 20uA current mirror since there is a N-MOSFET in between? 

* Is this controller suitable to be used in this topology? so far I didn't have any luck with the simulation. Any other recommended controller?.

Thanks in advance.