Post Go back to editing

Power on time delay

Category: Hardware
Product Number: MAX17614, MAX1761

Hello I have the following questions on MAX17614:

  1.  I'd like to request developing MAX17614 model available in LTspice – I could only find MAX17613A/B/C from library.
  2. By comparing the datasheets between 17614 and 17613, I found 17613 has 16ms of “Reverse Current Blocking Powerup Blanking Time” – does it mean the power on will have 16ms delay inherently? By simulation, I do see it (shown below, I just used the datasheet given circuit and try out without any load – while the input reaches 24V by 1ms, the OUT doesn’t rise up until ~16ms.), so I just would like to double-confirm with ADI.
  3. How about 17614? I don’t see the same Blanking Time from the datasheet, so does it mean it won’t have this delay when power on?

 

thanks!

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.