KCC's Quizzes AQQ304 - A pure logic
1. Quote of the month: "I am not lazy, I'm just in energy-saving mode" - unknown
2. Quiz AQQ304 about finding a pure logic puzzle
Mike is looking at Anne, but Anne is looking at Paul.
Mike is married, but Paul is not.
Question:
Is a married
View All
September Monthly Blog Quiz! Read the blog, take the quiz, and you could win a gift card
Quiz: How Well Do You Know Adaptive Power Switching?
Is your I/O module overheating? The AD74416H's Adaptive Power Switching (APS) can cut heat dissipation by up to 40% — but how well do you really understand how it works?
Read the blog first: Cooling
View All
LTC4290
Production
The LTC4290/LTC4271 chipset is an 8-port power sourcing equipment (PSE) controller designed for use in IEEE 802.3at Type 1 and Type 2 (high power) compliant...
Datasheet
LTC4290 on Analog.com
Dear Sir,
We are using the LTC4290AIUJ/LTC4271IUF (Auto mode) as our PSE controller.
When we plug in a Class 2, 3, or 4 PD device,
the PSE port status register always reports the device as Class 4, regardless of the actual PD device class is 2/3/4.
then measuring LTC4290A output port voltage event. event is 3 finger.
may i ask way? this event finger not meet datasheet power on sequence.
The waveform we measured at below. thanks.
Class 2 PD device:

Class3 PD device:

Class 4 PD device:

LTC4290 datasheet power on sequence:

Have you confirmed the PDs are drawing the correct class currents for Class 2, 3 and 4 during the first class event?

The three waveforms show a similar voltage for the first class event. This could mean each PD is presenting a Class 4. But the difference can be very subtle and reading class current is the only sure way to determine this.
Please provide a waveform of the current to the PD during classification.
If a current probe is not available, a DC voltage of 18V can be applied to the PD on Ethernet pairs 1/2 and 3/6 by splicing Ethernet cable.
Dear Sir,
i will check the current to the PD during classification. maybe use DC voltage of 18V can be applied to the PD on Ethernet pairs 1/2 and 3/6 by splicing Ethernet cable. then check DC source current.
but, why classification have 3 finger? i have use LTC4278 PD device board to test. then LTC4290A output port classification is 3 finger.
Dear Sir,
i will check the current to the PD during classification. maybe use DC voltage of 18V can be applied to the PD on Ethernet pairs 1/2 and 3/6 by splicing Ethernet cable. then check DC source current.
but, why classification have 3 finger? i have use LTC4278 PD device board to test. then LTC4290A output port classification is 3 finger.
If the LTC4290A/LTC4271, set in Auto mode, sees a Class 4 on the first class event, it will proceed to two additional class events. If the controller see a Class 0, 1, 2, or 3 on the first class event, it will proceed to power on the device without the additional class events.
Since the claimed Class 2 and Class 3 PDs are resulting in three class events, this indicates these PDs are not properly providing their respective Class to the PSE and appear a Class 4.
If the LTC4290A/LTC4271, set in Auto mode, sees a Class 4 on the first class event, it will proceed to two additional class events. If the controller see a Class 0, 1, 2, or 3 on the first class event, it will proceed to power on the device without the additional class events.
Since the claimed Class 2 and Class 3 PDs are resulting in three class events, this indicates these PDs are not properly providing their respective Class to the PSE and appear a Class 4.