Post Go back to editing

MAX6460 Simulation model

Category: Datasheet/Specs
Product Number: MAX6460

I have a couple of questions regarding the MAX6460 simulation model, where the simulation model behaves different from what I would have assumed looking at the datasheet. I am planning to use the chip as an overvoltage detector. So Ref connects through a voltage divider to the In- pin and the voltage I am monitoring is connected through a voltage divider to the In+.  

  • It appears that the reference voltage at the ref pin is around 1.32V, while according to the datasheet it should be around 2.25V 
  • It seems like the In+ pin clamps the voltage to the reference voltage. Is this how the actual chip will also behave? 

Thread Notes

Parents
  • Hi  ,

    Do you have test schematic that shows these results? I would suggest zipping up your schematic files uploading to this thread, and also report the problem here.

    mike (LTspice Team)

  • Hi Mike, 

    Thank you for your response. I am using ngspice (with KiCad) for simulation. But I am pretty confident the behaviour could be replicated in LTSpice. This is my test circuit which is close a circuit from the datasheet (page 9). 

    The output I am getting is as follow: 

    The following is not what I expect: 

    - I would have expected "ref" to be 2.25 V

    - I would have expected V(in-) to be the input negative input of the comperator, instead it seems it is "ref"

    - I didn't expect that V(in+) to be clamped slightly above (Vin-)

Reply
  • Hi Mike, 

    Thank you for your response. I am using ngspice (with KiCad) for simulation. But I am pretty confident the behaviour could be replicated in LTSpice. This is my test circuit which is close a circuit from the datasheet (page 9). 

    The output I am getting is as follow: 

    The following is not what I expect: 

    - I would have expected "ref" to be 2.25 V

    - I would have expected V(in-) to be the input negative input of the comperator, instead it seems it is "ref"

    - I didn't expect that V(in+) to be clamped slightly above (Vin-)

Children
No Data

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.