Post Go back to editing

problems with operation and I2C

Category: Hardware
Product Number: LTC3350

Hi.

This is my first design with the LTC3350.

I have several problems.  The first one is related to I2C. According to the datasheet, the address for communicating with the controller is 0x09, but in reality, after several hours, I scanned all the addresses on my bus and found that the LTC3350 responds at address 0x79. (I only have this device on the I2C bus).

Using this address, I have been able to read all the registers and it works correctly. (I can see the correct voltages in VIn, number of Caps, etc...)

On the other hand, neither the capacitor charging (360F) nor the step-up are working for me.
With the capacitors discharged (or charged), I supply 12V and it does not charge.
I remove the input power supply, and the controller does not generate the 12V output

This is my schematic.

On the TGATE pin, I see spikes only when cutting the input power, but it does not regulate to the programmed output voltage (12V).

Any idea where the controller problem might be and why it communicates with address 0x79 instead of 0x09?

Thank's a lot.

  • The supercapacitors are on a separate PCB (Includes the balancer).

  • Hello,

    Thank you for your questions. Interesting about the I2C address. The IC is set with the 7-bit address of 0x09 with the W/R bit (0x12 and 0x13). I have not ever heard of the I2C address being a problem previously. 

  • Hello,

    Thank you for your questions. Interesting about the I2C address. The IC is set with the 7-bit address of 0x09 with the W/R bit (0x12 and 0x13). I have not ever heard of the I2C address being a problem previously. Maybe there is a noise issue because of layout or something. It might be good to look at some scope shots on the I2C.

    The schematic looked OK. The PFI falling threshold should be set above the VCAP set voltage. For a design where the OUTFET is not needed, C48 can be decreased a little, maybe 4.7nF. 

    I do not see anything obvious from the schematic that will cause this issue. Is it possible to get a scope shot of the startup with VIN, SW, and /PFO?

    How closely were the PCB layout recommendations followed in the datasheet? Is it possible to also share the layout?

  • Hi Marty.

    I have readjusted the PFI and CAPFB dividers so that PFI is bigger than CAPFB. (But it still does not work.).

    PFI adjusted at 10.81V,   and CAPFB=10.14V.

    I am attaching the screenshots of PFO and SW.

    VIN (CH1) / PFO (CH2) on Falling Vin.

    VIN (Ch1) / SW (ch2)

    And the PCB Layout: (4 Layers.  Layer Stack: GND, GND, GND, VIN)

    This is the I2C bus reading of the LTC3350 registers: (in case it helps with anything)

    Thank's a lot.

  • Hello.
    I'm still unable to make any progress.
    Any ideas?

    Thank's a lot.

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.