Post Go back to editing

Max. Capacitive Load

Category: Datasheet/Specs
Product Number: MAX14521E

Hello, I need to connect 50nF electroluminiscence foil to one output (EL1). It is OK please? 

"An RSN value of 20Ω and CSN value of 330pF is sufficient
for VDD < 5V and CLAMP_TOTAL < 40nF. For
higher capacitive loads on the EL output or for VDD > 5V,
CSN must be increased to keep LX spikes less than 30V."

Regard to this text from datasheet...If I can connect 50nF to one output, which capacity of capacitor CSN must be please?

Thank You

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.