Post Go back to editing

Hot swapping Parallel Batteries of Different Voltages

Category: Hardware
Product Number: LTC4260

Hello dear community members,

I am new to this space so I apologise incase if something is not properly followed.

I am building a circuit that can be used for hotswapping of parallel Li-ion battery packs, nominal voltage of 48V. The aim is that the higher battery should charge the lower voltage battery with a constant currrent of 20A untill both batteries can safely power the DC Bus.

I am exploring the options of Hotswap and Current Limiting ICs like the LTC4260 by Analog Devices and I have the following questions / concerns.

  1. My concern is that if both sides are active loads like battery, if one battery is at relatively higher potential than the other one let say Batt 1 is 60V, Batt 2 is 44V and internal resistances of both batteries are 8 milli-Ohm respectively. In normal case the inrush current can be in Kilo Amperes due to high voltage and low internal impedance. Can the LM-5066 or similar IC be used safely for this use case ?

  2. I also want to understand whether it is a good idea to use this type of topology or should I design with a buck convertor method. Because for PoC I am trying to build a 5A Current Limiter with LTC4260 and MOSFETs, where the heat dissipated across MOSFET is coming around 75W.

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.