I'm using the MAX25256ATBAV+T chip to power the gate driver.
Of the many boards I've built, one or two generate intermittent fault signals.
The datasheet states that the fault signal is generated when the board is OCP or OTP, but my board only allows up to 75mA to flow, even when malfunctioning.
Could other factors, such as input power quality, affect the fault signal generation?
Also, when building this board, the temperature reached 260.4°C during reflow soldering.
The datasheet states that the reflow soldering temperature is up to 260°C, but can exceeding that by even 0.4°C cause the fault?
The fault signal is generated immediately upon power-up and remains unrecoverable without a reboot.
Edit Notes
Language errors[edited by: nobleman at 4:46 AM (GMT -4) on 7 Aug 2025]