Hello,
I am designing a buck led driver circuit, specifications are:
- Input 48V
- Output current max 14A
- Output Voltage 32-35V
I was looking for MAX20078 since it has external mosfet (so no current limitations) and analog diming. Unfortunately I have seen in another topic that beyond 10A there may be ringing on the LX node.
What output current is possible with the MAX20078 LED Driver?
Can you suggest me a specific circuit configuration? Or alternatively a different PN ?
Is there an LTspice model for this component?
Thank you,
Enrico