Post Go back to editing

LT3081 Parallel Configuration for Laser Diode Drive

Thread Summary

The user is configuring multiple LT3081 linear regulators in parallel to power a laser diode (1.8 V, up to 9 A). The final answer confirms that the regulators can be used as current sources in parallel, but the output voltage must be set externally using the SET pin and resistors. If the SET pin is grounded, the output voltage will be the minimum allowed. The regulators will not force a higher voltage if the load does not require it, and thermal dissipation is manageable with the given parameters (1 W at 1.5 A).
AI Generated Content

Hi,

I'm working on powering a laser diode (1.8 V, up to 9 A) by paralleling multiple LT3081 linear regulators. My plan is to use three LT3081s in parallel to deliver up to 4.5 A (1.5 A per LT3081), and potentially more if needed. I’ve set this up in LTspice, and I’ve attached a screenshot and the simulation for reference (please disregards voltage sources at 0).

In my circuit, I’m using a potentiometer at R4 to adjust the current limit, and another at R11 to set the output voltage.

I have a couple of questions regarding the behavior of these potentiometers: I have read that you can ground the SET pin, so If I remove R4 and R3, will the LT3081 automatically set the output voltage based on the load demand? In my case, the laser operates at 1.8 V - would that voltage be maintained?

Since laser diodes are current-driven devices, how critical is the voltage setting at the SET pin? In the simulation, I set the output voltage to around 1.9 V to prevent overdriving the laser. However, I'm concerned - if I accidentally set the voltage too high (e.g., 3 V), would the LT3081 try to force that voltage and potentially damage the laser? By the way, in the simulation when the SET is to ground, the simulation does not work properly.

I also read in the documentation of the LT3081 that it can be configured as current source, but I am not sure if they can be paralleling or how to achieve it and if thermals will be problematic for the current I would like to get.

Any guidance would be greatly appreciated.

Thanks!

 3731.LT3081_TA01A_triplecurrreg.asc

Thread Notes

Parents
  • I attached an image of one way to make a current source for a 9A LED that is controllable with a digital potentiometer.  I am a little busy these days, so I probably won't be able to engage further, but my advice is to make a clear, realistic specification for what you want to accomplish and start with a reference design that you can adapt to your needs.    

    LT3083 9A curr source_2.png

  • Thank you so much for your feedback, much appreciated! I will start with your suggestion. Just wondering why the approach I made is wrong or not appropriated for my design, I know that current source is the most appropriate for laser, but the one I made could also work? and no worries, any time you could have in future to give me more insights on this will be much appreciated.

    Oh, I also realized that your approach is using LT3083. I was interested to use the LT3081 because of the current and temperature monitoring capabilities.

Reply
  • Thank you so much for your feedback, much appreciated! I will start with your suggestion. Just wondering why the approach I made is wrong or not appropriated for my design, I know that current source is the most appropriate for laser, but the one I made could also work? and no worries, any time you could have in future to give me more insights on this will be much appreciated.

    Oh, I also realized that your approach is using LT3083. I was interested to use the LT3081 because of the current and temperature monitoring capabilities.

Children
No Data

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.