Post Go back to editing

one phase LTC7871

Category: Hardware
Product Number: LTC7871

Hi everyone, I only need to use one phase of the LTC7871 during calibration.

Can I tie the SNSA+, SNSD+ & SNS- pins together  and connect the combined traces to VLOW with a low-RON analog switch (eg ADG5433)?

Many thanks in advance

I.C.

  • Hello I.C.,

    The LTC7871 can be used with just one phase. But, could you give me more details on your circuit. For instance, do you intend to use all 6 phases during normal operation and use just one in calibration? Why are you using an analog switch? 

    If you wish to temporarily disable a phase and the LTC7060 is being used, then a phase can be disabled by tying the EN pin of the respective LTC7060 to GND.

    Best regards,

    Mike

  • Hi Mike, I read in another thread that to disable the LTC787X's phase, I need to connect the SNSA+, SNSD+, and SNS- pins together with VLOW. Otherwise, if I could just disable the respective MOSFET driver, the schematic would be easier to implement.

    thank a lot

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.