Post Go back to editing

Query regarding the capacitor values at 'Vc' pin of LT83203

Category: Hardware
Product Number: LT83203

I am utilising the LT83203 to convert a 12V input supply to 1.7V output supply.


The capacitor connected to the Vc pin (Cc) is 3.6 pF for my design. 

But, due to unavailabiltiy of this capacitor, I'm thinking of using the 3.3 pF or 3.9 pF ones (these two are available). 

Which one of these capacitors should I go for so that my output voltage remains relatively the same?

What are the implications of this capacitor in the working of this IC? I do know that this pin is connected to the error amplifier output, but how exactly are we compensating the control loop using this RC Network at pin 'Vc'? 

Please do share your valuable insights.