Post Go back to editing

ADP5091 > how to select minop resistor?

Thread Summary

The user asked how to select the MINOP resistor for a circuit. The final answer explained that the MINOP pin is driven by a 2 microamp current source and the resistor value should be set using V = IR to determine the shutdown voltage of the energy harvesting source. The example circuit in the data sheet uses a 150k resistor, resulting in a 0.3V shutdown threshold for PV cells with 0.7-1.1V open-circuit voltages. The accompanying answer clarified that connecting the MINOP pin to Vref was unnecessary and overcomplicated.
AI Generated Content
Category: Hardware
Product Number: ADP5091

I'm trying to figure out how to select the minop resistor, could you please help? point to AN/Doc?

  • I haven't used this part myself; below is my best guess

    after reading through the data sheet.

    The MINOP pin is driven by a 2 microamp current source,

    and the voltage of the MINOP pin is sensed to determine

    minimum operating voltage of the harvested source as

    seen at the Vin pin.

      

    For example, consider Figure 45, one of the Typical

    Application Circuits in the data sheet. The MINOP

    resistor is 150k, so 150 kOhm * 2 microamp = 0.3V.

    As noted in the footnote, the circuit is designed

    for PV cells with open-circuit voltages in the

    0.7-1.1V range. The designers apparently decided

    that if the ambient light level is so low that

    the voltage of the cell drops to 0.3V, it is best

    to shut down.

    For your own application, you would have to

    determine the appropriate shut down voltage

    given the energy source you are harvesting,

    and then use V = IR to set the resistor value.

  • thank you for this clear description, I wish the DS was it.

    And, sometimes it is easier that we think, I was confused and tried to get the source for 2uA... I was trying to connect it to Vref... and all got too complicated.

    But, the way you list it :) it is nice and clear.

    thank you!

    wishing you a good day!