I have a issue about the thermal shutdown of Max22205. The Irms of H-Bridge is 4A rms. Currently, I measure the current is under 1A, but the temperature of body is over 100C. How can I reduce the thermal? BTW, the package is TTSOP.
MAX22205
Recommended for New Designs
The MAX22205 integrates a high current 65V, 7.6AMAX H-Bridge to drive one Brushed DC motor or one half Stepper motor. The H-Bridge FETs feature very low...
Datasheet
MAX22205 on Analog.com
I have a issue about the thermal shutdown of Max22205. The Irms of H-Bridge is 4A rms. Currently, I measure the current is under 1A, but the temperature of body is over 100C. How can I reduce the thermal? BTW, the package is TTSOP.