Post Go back to editing

LT3083EQ#PBF Output 0.3V 6A

Category: Hardware
Product Number: LT3083EQ#PBF, LT3083

I want LT3083EQ#PBF to output 0.3V 6A. My schematic is like this, but the output voltage is 2.2V. What is the problem?

  • The LT3083 doesn't have a ground pin, so the quiescent current must exit the device through the OUT pin.  In other words, the LT3083 will have high output if the minimum load requirement is not respected.   I show some references from the datasheet in the image below.    

    LT3083 DS preload R and min load_2.png

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.