Post Go back to editing

LTM8063 Operating Temperature

Category: Hardware
Product Number: LTM8063

Hi all,

Very little current (approximately 100 mA at 15 voltage from output) is drawn from the LTM8063's output, but the integrated circuit does get hot. Within a few minutes, the integrated circuit temperature rises to 75 degrees and I could not understand why the integrated circuit is so hot. Is this normal? I shared my design paremeters. What solution do you suggest to reduce the integrated circuit temperature? Are there any errors in the design?

VIN: +28VDC

VOUT: +15VDC

LOAD CURRENT: 100mA

RT: 18.2Kohm

FB: 13.5Kohm

Ambient Temperature: 25C

Thanks,

Bulent