I am trying to power 2 AD811 op-amps using the MAX629 set to output at -15V. Using the specified circuit in the datasheet of the regulator and the recommended components, I managed to get the regulator to output at -12V but the regulator fails under a load greater than 17mA when it is specified for 500mA and the voltage drops to -2 V.
I have included an image of the schematic I implemented on a PCB. Mind that the inductor name may not match the specification but I am using a 47µH power inductor with a large enough current rating. The diodes are the MBR0540L, and the capacitors are rated to 50 V.
I am seeing ringing at the LX pin when I probe using a short ground lead scope that is probably messing with the feedback and causing oscillation, but I have not been able to identify what is causing the problem exactly. Any help would be appreciated.