Post Go back to editing

Power Management

Category: Hardware
Product Number: LTC4263

Dear All,

I'm planning to use LTC4263IDE#PBF for IEEE802.3af Class2 power management.
I plan to use 4 circuits in parallel. Referring to Figure 5 on the datasheet, I connected all the PWRMGT pins, set RPM to 7.68kΩ, and CPM to 1uF.


As a result, PoE power is supplied for one device, but when four devices are connected, only one is powered.
Using the RPM formula, I calculated 7.68kΩ as 213kΩ/(7W×4).
Is this wrong?

As additional information, the PoE classification waveform is Class2, 15.6V. If anyone has any information, please reply.

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.