Post Go back to editing

MAX26240 vs. LTM8054 for 20 V @ 3 A Boost from 10–30 V Input—What Am I Missing?

Category: Datasheet/Specs
Product Number: MAX26240

Hi folks,

I need to generate a 20 V, 3 A output (≈60 W) from a 10–30 V input rail and I’m trying to keep the design as compact and cost-effective as possible. I’m torn between two solutions:

  • LTM8054 µModule

    • Fully integrated power stage + controller + passives

    • Handles up to ~75 W

    • Small footprint but costs around $50

  • MAX26240

    • High-frequency boost controller with integrated MOSFET

    • Requires a few external inductors, diodes, and capacitors

    • Non-BGA package makes hand-soldering easier

    • Only about $7 in single-unit quantities

The price difference is huge, and the MAX26240’s non-BGA package plus minimal extra components look very attractive—if it really can deliver 20 V @ 3 A. But I’m worried:

  1. Integrated MOSFET capability: Can the MAX26240’s built-in switch really handle ~60 W continuously, or will thermal and R<sub>DS(on)</sub> limitations kill efficiency/require heavy heatsinking?

  2. Hidden trade-offs: Are there layout or EMI headaches, worse dynamic response, or other gotchas compared to a µModule solution?

  3. Feature gaps vs. LTM8054: Apart from price and package, what major differences in protections, efficiency, external component count, or thermal performance should I be aware of?

Has anyone used the MAX26240 (or similar controllers) in a 50–75 W boost design? Did you run into limits that forced you to switch to a fully integrated module like the LTM8054? Any pointers or alternative IC recommendations would be greatly appreciated!

  • Merhaba Codeerrzz,

    Without going to the too much details, a uModule is an highly integrated solution. You can buy one EVKIT/sample and test quickly how it functions.
    This is the fastest way, that you have a working system on your hand. uModules are unbeatable or this.

    If you have resources  and time, you can consider designing a discrete design then as you mentioned with MAX26240.
    A discrete design has always many additional design steps and more time need, since you do the electrical layout, thermal management, EMC compatibility, BOM manangement etc. yourself.

    P.S. What you do is Buck-Boost converter, not a pure boost, since your Vout (20V) lies in the Vin range (10....30V). 

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.