LTC3890
Recommended for New Designs
The LTC3890 is a high performance dual step-down switching regulator DC/DC controller that drives all N-channel synchronous power MOSFET stages. A constant...
Datasheet
LTC3890 on Analog.com
Hi All,
I have noticed that the power good (PG) pin is misbehaving when powering up the IC from EXTVCC.
The sequence is as follows:
If you then turn on VIN, PG goes low during the soft-start and then high after the output voltage is within 10% of VOUT. This is as expected.
If you now turn-off everything and repeat the sequence above right afterwards, the PG stays low. When measuring the resistance PG to GND while everything is off (after the IC ones hat VIN supply) the PG FET seems to be still on (50Ohm to GND). Only after multiple hours the internal FET seems to turn-off.
Could you please confirm whether the internal FET has an active pull-down on the gate? If not, the behaviour would make sense and we would stop investigating it.