Post Go back to editing

Urgent Assistance Required : LT3032EDE-5 Negative output Issue

Category: Hardware
Product Number: LT3032

Hi

I have developed a project using the  LT3032EDE-5 Linear regulator . The positive output side is functioning correctly , delivering +5 V as expected. however, I am consistently observing  -6V on the negative output side instead of expected -5V.

This issue persists even when replicating the circuit on the general purpose board. As we are approaching the final production phase, this issue is preventing us from proceeding to manufacturing.

I Would be greatly appreciate any guidance or recommendations you can provide to help resolve this matter promptly.

Thank you for the support.

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.