Hello,
I would like to use the LT3042 to generate a low noise ( <10uVRMS at BW 10Hz->100kHz) rail of 2.5V nominal with +-200mV trimming capability (2.3V to 2.7V).
I was thinking of implementing the circuit by using a 22.9kOhm 0.1% (2.29V output) precision resistor in series with a 470Ohm multiturn trimmer used as a variable resistor
My main doubts with this solution are:
- The poor charateristic of the pot will introduce too much noise and instability (TC)
- It becomes more difficult to guard the SET signal on the PCB due the big size of potentiometer and it will for sure degrade noise perfomarce
The second implementation i tought of is by using an external reference that has TRIM capabilities (like MAX6225) but the range is usally smaller (+- 25 or 50mV)
Thanks for the help.