Post Go back to editing

LTM4668A strange behaviour in dual mode

Category: Hardware
Product Number: LTM4668A

I have problem with LTM4668A witch such configuration:

VCC_3.3v works correctly but VCC_2.5V not. There is 2.82V and on POWER_FB_VCC_2.5V i have 0.7V. 

Both power En works very strange. Both OFF -> 0V on both output but activating one of them activates both Outputs. 

I have changed C390 to 4u7 and this is the oscillogram:

POWER_FB_VCC_3.3V -> ~13.4kR

POWER_FB_VCC_2.5V -> ~20kR - changing this value, VCC_2.5V doesn't change. 

Same situation on three boards. 

Simulating this circuit in LTspice seems to work fine.

Any suggestions?

There is an issue on the schematic? or what should i check/ measure to understand what is happening there. 

Edit Notes

.
[edited by: Matt00 at 6:55 AM (GMT -4) on 26 May 2025]

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.