Post Go back to editing

MAX20075D Skip mode current threshold

Category: Hardware
Product Number: MAX20075D

Hi, the datasheet for the Max20075D says this about Skip mode: 

"Skip mode is entered when the SYNC pin is connected to ground or is unconnected and the peak load current is < 150mA (typ)."

I cannot see a load current range in the datasheet. What are the max/min values for this threshold? 

Thank you.