Could you please let me know the value of the internal feedforward capacitor (Cff) in the LT8607-5?
I would like to use it with adjustable LT8706 version when simulating in LTspice or LTpowerCAD.
LTspice
Production
LTspice® is a powerful, fast, and free SPICE simulator software, schematic capture and waveform viewer with enhancements and models for improving the simulation...
LTspice on Analog.com
LT8607
Recommended for New Designs
The LT8607 is a compact, high efficiency, high speed synchronous monolithic step-down switching regulator that consumes only 1.7µA of non-switching quiescent...
Datasheet
LT8607 on Analog.com
Could you please let me know the value of the internal feedforward capacitor (Cff) in the LT8607-5?
I would like to use it with adjustable LT8706 version when simulating in LTspice or LTpowerCAD.
LT8706 was a mistake. I would like to simulate the LT8607-5 using the adjustable LT8607 model and the internal Cff value.
LT8706 was a mistake. I would like to simulate the LT8607-5 using the adjustable LT8607 model and the internal Cff value.
Hi,
Thank you for your reply.
According to the pin functions description, VOUT is connected to an internal 6.6 MΩ divider. So, assuming the same time constant as the 1 MΩ // 10 pF combination in the adjustable version, would the internal capacitor be more like 1.5 pF rather than 10 pF?