Greetings!
I have a problem setting up my MPPT, I have an input solar pannel of 14V and I want to use the LT8491 it as a 22V output battery charger. Still, when performing the connections, I receive 0V on the output. I checked the enabled pin in the SWENO, but it seems disabled. We also tried connecting the battery to see if this triggers the MPPT IC as we read in one forum (the IC won't give voltage until it senses the battery). I attached the schematics, I hope to receive some insights from you. Thank you so much in advance!