Post Go back to editing

LT8653S package corner pads versus DC2535A

Category: Hardware
Product Number: LT8653S

In a previous design I used the LT8609S which has corner pads shown in the datasheet as well as on the DC2522A paste layer.

I'm laying out a design using the LT8653S which has corner pads shown in the datasheet (page 30 drawing marked LTC DWG # 05-08-1524 Rev C), however I don't see them in DC2535A pdf artwork so I'm unclear if those pads are physically present on the actual device.

Does the LT8653S have corner pads similar to the LT8609S which should be soldered to the PCB?