I'm using a MAX17502H DC-DC converter for converting 5 V to 3.3 V, as per the calculation inductor value is 24.75 μH, but I used a 22 μH inductor because of component availability. Problem is output voltage is not generating for 5 V input supply, output voltage is generating only above 5.3 V input supply voltage. I'm not able to figure out what the issue is, or what I can do to get 3.3 V output for 5 V input supply voltage.
Please find attached schematic for reference and datasheet link.