The datasheet of the MAX17291B tells that the maximum output voltage of this module is 20V. I would like to supply variable output voltages that I configure using a PWM input signal in the module. I would like to get voltages that range between 5-30V
In the following image of the LTSpice simulation I can achieve this 30V output voltage. Would this be possible in real applications?