Hi,
I'm working on a new application using nPM1100 PMIC for power management and LTC2950-1 as a push-button controller to try to implement device ON-OFF and SOS functionality using single Tactile/Push Button Switch.
However, the push-button circuit is not working as expected. The board gets hot, and the VSYS voltage drops to around 1V when connected to a 5V USB supply. When I removed the push-button circuit block, everything works fine.
I'm sharing the implemented circuit and the reference schematics I followed. Could anyone help debug the issue?
Thanks in advance.
For more details, kindly check the post link below:
Implemented:

Reference Circuit: