Hello:
Need a fast resolution: can we do a step up converter using LTC 3765 & LTC3766 controllers?
Input: 22 to 32VC DC or can have it boosted to 200V using another module with isolation such as AC Flyback- which has isolation.
Wont really want to have 2 isolation transformers.!
Output: 100v
power : 300 W
Since there is a transformer, is there anything topologically impossible with 1:N step up conversion? Apart from the PMOS, will be using all GaN devices.
Will appreciate a fast resolution of this..-
-Boiugnoul