Post Go back to editing

LT8364 SEPIC bad output voltage

Category: Hardware
Product Number: LT8364

Hello everyone, I need help with the LT8364 power supply in the connection according to the datasheet page 24. It is a 5V SEPIC power supply, I need about 100mA. I have a 47ohm resistor connected as the output. I have one test piece assembled on a double-sided board and it works without problems. I have the second piece with the same connection and the same values ​​on a single-sided board and a different layout. However, this connection does not want to work properly. It does not reach the output voltage. I attach the input and output voltage curve in a graph. Can anyone please tell me whether the layout of the components on the board has such a fundamental impact on functionality? Or other advice. Thank you.U in vs U out

Schema

Thread Notes