KCC Quizzes AQQ303 about the radius of a circle
1. Quote of the month: "When I die, I want to die like my grandfather who died peacefully in his sleep. Not screaming like all the passengers in his car" - Will Rogers
2. Quiz AQQ304 about finding the radius of a circle
Good luck, and try to be
View All
August Monthly Blog Quiz! Read the blog, take the quiz, and you could win a gift card
Important: Read the blog first . The quiz questions are all based on the content of the blog:
Stay in the loop and win! Read the blog Current Output Driving Industrial Loops , then take our quick five-question quiz for a chance to win a gift card
View All
LTC3862
Production
The LTC3862 is a two phase constant frequency, current mode boost and SEPIC controller that drives N-channel power MOSFETs. Two phase operation reduces...
Datasheet
LTC3862 on Analog.com
Hello,
I have designed a boost converter using the LTC3862 that goes from 24V to 110V and produces 1.8A (200W).
It seems to be oscillating at around 1.3kHz, with the ripple being a few volts on top of the 110V nominal output voltage.
I used LTpower cad for the initial compensation values. As I don't have a network analyzer what would be the best way to adjust the compensation values?
Thanks;
Leo
Here is the starting point.