I am using the MAX5971A PSE controller in my project with a Raspberry Pi CM4 to power a Basler aca 1300-60gm NIR IP camera. However, the camera is not powered on. I have verified that the 54V power supply to the PSE controller is present. I am using a 54V isolated DC-DC Converter (PKE3316) for the power supply.
I have attached the schematic for reference. Could someone please review the connections and let me know if there are any issues? Kindly advice on any debugging steps that can be taken to troubleshoot this issue. Any help would be greatly appreciated!