Post Go back to editing

Externally programmable current limit when paralleling multiple LT3091/LT3081

Category: Datasheet/Specs
Product Number: LT3091

Hi,

I'm trying to figure out how to program the external current limit for multiple LT3091/LT3081 connected in parallel.

From the LT3091* datasheet I can see that it is possible to use a single common resistor to program the current limit of all the regulators. However, I am unsure how to modify the R_ILIM equation to account for multiple LT3091* in parallel. Any help you can provide would be greatly appreciated. 

Any help you can provide would be greatly appreciated.

/
Any help you can provide would be greatly appreciated.

/

For the LT3081*, it appears that each regulator should have its own R_ILIM resistor. With a programming scale factor of 20 kOhm A, each LT3081 will need a 20 * N / I_LIMIT kOhm resistor (with I_LIMIT being the total maximum current and N the number of regulators). Is this right? Would it be possible to use a single common resistor to program the current limit of all regulators also for the LT3081*?

Thanks. Best regards,
Andrea

(*) As pointed out by ARad, I have swapped the part numbers of the two regulators.

Edit Notes

(Added a note to avoid confusing anyone reading the post.)
[edited by: andreaiob at 10:19 AM (GMT -5) on 27 Feb 2025]

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.