Hi!
Can you suggest an optimal layout for SEPIC -24V from the LT8344?
I am struggling with best placement for minimsing the hot loop.

| SLA Status | Assignee | Support Status |
|---|---|---|
| ⚠ 13184 hours | Closed | |
LT8334
Recommended for New Designs
The LT8334 is a current mode DC/DC converter with a 40V, 5A switch operating from a 2.8V to 40V input. With a unique single feedback pin architecture,...
Datasheet
LT8334 on Analog.com
Hi!
Can you suggest an optimal layout for SEPIC -24V from the LT8344?
I am struggling with best placement for minimsing the hot loop.

Pity there's no suggested layout in the datasheet. I see you have a picture of the component placement from the Demo Manual though.
All I can suggest is to look at the datasheet for the LT8711 Micropower Synchronous Multitopology Controller with 42V Input Capability. It has layout suggestions for all the different topologies.
There's a SEPIC converter evaluation board and you can download the gerbers for it.
I have selected a non-coupled layout using
Cin 2pcs 4.7uF X7R 1206 - TDK CGA5L3X7R1
L1,2 2.2uH IHLP2525
D1,2 B340AF
Ccouple 2pcs 4.7uF X7R 1206 - TDK CGA5L3X7R1 ( top & bottom )
Ccatch 2pcs 0.1uF X7R 0402 - MUTATA GCM155R71
Cbulk 2pcs 22uF X7S 2220 - TDK C5750X7S2A
The -30V loop could be shorter.