Post Go back to editing

About the internal power MOSFET

Category: Datasheet/Specs
Product Number: LTC4267

Hello team,

Under the conditions that the switching regulator of LTC4267 works normally(PWM enabled),
if an overcurrent flows on the secondary side(POE) and a current through the VPORTN
exceeds 350mA, will the current be limited to 350mA by controlling the FET shown below?

Best regards,

  • Hello,

    Sorry for the delayed response. Assuming we are considering current flowing in the conventional direction (POUT to VPORTN), then yes, the current will be limited to 375ma (typical). The PD interface includes dual level input current limit. At turnon, before the POUT load capacitor is charged, the PD current level is set to a low level. After the load capacitor is charged and the POUT – VPORTN voltage difference is below the power good threshold, the PD switches to high level current limit. The PD stays in high level current limit until the input voltage drops below the UVLO turn-off threshold.

    Best Regards,

    Eric

  • Hello Eric,

    Thank you very much for your reply.
    I have inferred that the current was limited to 375mA from the Input Current Limit section on page 13 of the datasheet, but your response clarified that.

    Thank you and best regards,
    Tsuyoshi Tokumoto

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.