Hello
Can I operate the LT3080 as below:
Vin = 4.2V ,
Vcontrol = 12V
Vout = 3.6V
output current max. = 500mA. , Is this ok?
Roi
KCC Quizzes AQQ303 about the radius of a circle
1. Quote of the month: "When I die, I want to die like my grandfather who died peacefully in his sleep. Not screaming like all the passengers in his car" - Will Rogers
2. Quiz AQQ304 about finding the radius of a circle
Good luck, and try to be
View All
August Monthly Blog Quiz! Read the blog, take the quiz, and you could win a gift card
Important: Read the blog first . The quiz questions are all based on the content of the blog:
Stay in the loop and win! Read the blog Current Output Driving Industrial Loops , then take our quick five-question quiz for a chance to win a gift card
View All
LT3080
Recommended for New Designs
The LT3080 is a 1.1A low dropout linear regulator that can be paralleled to increase output current or spread heat in surface mounted boards. Architected...
Datasheet
LT3080 on Analog.com
Hello
Can I operate the LT3080 as below:
Vin = 4.2V ,
Vcontrol = 12V
Vout = 3.6V
output current max. = 500mA. , Is this ok?
Roi
Hi. Yes, the LT3080 is o.k. for your conditions. We specify PSRR at 1V IN to OUT as I show in the image below because that IN to OUT voltage gives the most repeatable PSRR, but your circuit will still work.