Hi, good morning, I'm currently designing a Hi-Fi preamplifier. It will deploy an instrumentation op amp (INA ...) based balanced audio receiver (XLR input), among the other parts (single Vcc). In order to properly feed this stage, my requirements for the linear regulator are:
- Output voltage from regulator 33 - 36 Volt
- Max input voltage to regulator > 60 Volt
- Current capability 50mA at least (max current drawn by the XLR received is about 15mA, 6mA quescent)
- Low noise
- Good PSRR
The only regulator which fits those requirements - if I did not miss anything - seems to be the LT3012. (I had previously tried to fit the LT3055, which has lower noise. Nevertheless, it has max input voltage of just 50 Volt, which makes me uncomfortable. Output from transformer - rectifier is 42 Volt in fact, which just leaves 8 Volt margin in case of power line surge).
So, back to the LT3012, in the picture below you see my draft design (two channels). The LT3012 is almost perfect; just the declared noise (100uV) seems little bit on the high side. Hence my questions:
- I cannot see information on noise, in case of lower current draw than 250mA. Should I expect a noise decrease (from 100uV) due to my low mA application ?
- Can I reduce noise by adding a feedthrough 10nF capacitor across the higher resistor ? I did not find this mentioned in the datasheet.
- Can I reduce noise utilizing lower value resistors ?
- RC filter at the output ? (I understand this might impact stability)
- Last question, (not related to noise, sorry), is it advisable to deploy 0.22 Ohm resistor before the IN pin, still for sake of stability ?
These are my questions. Thank you so much in advance for your help !
Cheers
Matteo